Pressure Calculator & Conversion Chart
Convert millibars to kilopascals and vice versa by using Farnell's pressure calculator below.
Our mass conversion chart also provides you with the multiplier for these conversions so you can make them manually when necessary.
Pressure Conversion Calculator
Pressure Conversion Chart
| Starting | Multiplier | Ending |
|---|---|---|
| Atmosphere (atm) | 760 | Torr (Torr) |
| Atmosphere (atm) | 1.01325 | Bar (b) |
| Atmosphere (atm) | 101.325 | Kilopascal (kPa) |
| Atmosphere (atm) | 101325 | Pascal (Pa) |
| Atmosphere (atm) | 1.0332274528 | Kilogram per Square Centimetre (kgf/cm2) |
| Atmosphere (atm) | 14.69596432068 | Pounds per Square Inch (psi) |
| Torr (Torr) | 0.001315789473684 | Atmosphere (atm) |
| Torr (Torr) | 0.001333223684211 | Bar (b) |
| Torr (Torr) | 0.1333223684211 | Kilopascal (kPa) |
| Torr (Torr) | 133.3223684211 | Pascal (Pa) |
| Torr (Torr) | 0.001359509806316 | Kilogram per Square Centimetre (kgf/cm2) |
| Torr (Torr) | 0.01933679515879 | Pounds per Square Inch (psi) |
| Bar (b) | 0.986923266716 | Atmosphere (atm) |
| Bar (b) | 750.0616827042 | Torr (Torr) |
| Bar (b) | 100 | Kilopascal (kPa) |
| Bar (b) | 100000 | Pascal (Pa) |
| Bar (b) | 1.019716212978 | Kilogram per Square Centimetre (kgf/cm2) |
| Bar (b) | 14.50378911491 | Pounds per Square Inch (psi) |
| Kilopascal (kPa) | 0.00986923266716 | Atmosphere (atm) |
| Kilopascal (kPa) | 7.500616827042 | Torr (Torr) |
| Kilopascal (kPa) | 0.01 | Bar (b) |
| Kilopascal (kPa) | 1000 | Pascal (Pa) |
| Kilopascal (kPa) | 0.01019716212978 | Kilogram per Square Centimetre (kgf/cm2) |
| Kilopascal (kPa) | 0.1450378911491 | Pounds per Square Inch (psi) |
| Pascal (Pa) | 0.00000986923266716 | Atmosphere (atm) |
| Pascal (Pa) | 0.007500616827042 | Torr (Torr) |
| Pascal (Pa) | 0.00001 | Bar (b) |
| Pascal (Pa) | 0.001 | Kilopascal (kPa) |
| Pascal (Pa) | 0.00001019716212978 | Kilogram per Square Centimetre (kgf/cm2) |
| Pascal (Pa) | 0.0001450378911491 | Pounds per Square Inch (psi) |
| Kilogram per Square Centimetre (kgf/cm2) | 0.9678411053541 | Atmosphere (atm) |
| Kilogram per Square Centimetre (kgf/cm2) | 735.5592400691 | Torr (Torr) |
| Kilogram per Square Centimetre (kgf/cm2) | 0.980665 | Bar (b) |
| Kilogram per Square Centimetre (kgf/cm2) | 98.0665 | Kilopascal (kPa) |
| Kilogram per Square Centimetre (kgf/cm2) | 98066.5 | Pascal (Pa) |
| Kilogram per Square Centimetre (kgf/cm2) | 14.22335835237 | Pounds per Square Inch (psi) |
| Pounds per Square Inch (psi) | 0.0680458919319 | Atmosphere (atm) |
| Pounds per Square Inch (psi) | 51.71487786825 | Torr (Torr) |
| Pounds per Square Inch (psi) | 0.0689475 | Bar (b) |
| Pounds per Square Inch (psi) | 6.89475 | Kilopascal (kPa) |
| Pounds per Square Inch (psi) | 6894.75 | Pascal (Pa) |
| Pounds per Square Inch (psi) | 0.0703068835943 | Kilogram per Square Centimetre (kgf/cm2) |