AI at the Edge
New Paradigm for IoT Implementations
Artificial intelligence integration in Internet of Things systems has changed how data is processed, analysed, and utilised. For years, all AI solutions have been happening in the cloud, but edge AI now offers a possible solution with enhancements to efficiency, security, and operational reliability. This paper tries to delve into the intricacies of AI on the edge, trying to find out its constituent parts, benefits, and the fast-changing hardware environment that supports it.
The Evolution from Cloud to Edge AI
Traditionally, IoT devices have relied directly on cloud infrastructures for AI processing. Sensor data from edge devices is streamed to the cloud, where it is then subjected to analytics and inference processing. However, this is starting to be fraught with significant problems as IoT applications increasingly demand more real-time decision-making at the edges of the network. The amount of data involved, latency problems, and bandwidth constraints render cloud-based processing less workable for many use cases.
Enter edge AI, which brings processing power closer to the data source—within the IoT devices themselves. This shift reduces the need for continuous data streaming to the cloud and offers a type of real-time processing that is critical in many applications, such as autonomous vehicles, industrial automation, and healthcare.
Core Components of Edge AI Systems
Specialised hardware and software elements go into making up the AI at Edge. Some important abilities rest on top of an edge AI system, including capturing, processing, and analysing sensor data locally. The content usually making up an edge AI model includes:
- Hardware for Data Acquisition: Data capture would not have been possible without proper sensors integrated with processing units and memory to store the same. Modern sensors are embedded with inherent processing capabilities that can process preliminary filtering and transformation of data.
- Model for Training and Inference: Pretrained, use case specific models are needed on edge devices. Models can be trained according to the feature selection and transformation to optimise performance during a training phase due to limited computational resources that are available at the edge.
- Application Software: The software on edge devices triggers AI processing, typically through microservices that are invoked based on user requests; such software can include running AI models, probably with customised features and aggregations part of their design from the training phase itself.

Figure 1: AI at the Edge Workflow
Benefits of AI at the Edge
AI at edge holds many distinct advantages compared to traditional cloud models:
- Improved Security: With local processing, sensitive data is less likely to be breached in transmission to the cloud.
- Greater Operational Reliability: Edge AI systems have reduced dependencies on network connectivity. They work pretty well in conditions that offer intermittent or low-bandwidth connectivity.
- Flexibility: AI at the edges allows the personalisation of models and features according to specific application requirements, which is very important in very diverse IoT environments with very different requirements.
- Lower Latency: This approach reduces the time needed to process data and provide a decision to a minimum, a critical feature in real-time applications like autonomous driving or medical diagnosis.

(image source)
Challenges in Implementing Edge AI
While edge AI has several clear advantages, there are challenges to implementing these systems. Developing a machine learning model for edge devices means handling huge volumes of data, choosing the right algorithms, and optimising models to run on constrained hardware. For many manufacturers, especially those focused on high-volume, low-cost devices, this can be an investment prohibiting them from developing these capabilities from scratch.
This is where the demand for programmable platforms comes in. The industry is increasingly moving toward application-specific AI architectures that can scale across a wide power-performance spectrum. These architectures balance the need for special processing capabilities against the flexibility of general-purpose designs.
The Role of Specialized Hardware in Edge AI
With the growing applications of AI and machine learning comes the growing need for bespoke hardware, which can tackle the unique demands of these technologies. Traditional general-purpose processors—though very important for manufacturing economies and common toolchains—have shown a poor fit for special needs in AI, particularly neural network processing.
To fill this gap, semiconductor manufacturers are proposing AI accelerators that can drive performance without giving up the advantages of general-purpose families. Such accelerators are designed for parallel processing, required by neural networks, and offer a more efficient path to AI execution.
Parallel Architectures and Matrix Processors: These parallel architectures, such as those realised in graphics processors, are very effective for neural network training. Matrix processors, like Google's Tensor Processing Unit—a processor specifically made to accelerate matrix manipulation, which is a critical component of neural network processing—are designed this way.
In-Memory Processing: Another of the newer innovative approaches is in-memory processing, whereby the memory array itself is turned into a neural network through the interconnection of cells with variable resistors. That reduces bottlenecks in traditional memory access, thereby bringing about huge gains in terms of speed and power efficiency.
The Future of Edge AI: Innovations and Opportunities
With the continuous growth of the Edge AI field, so too do new technologies and architectures to take on increasing demands in AI processing. One such prominent development is the rise of Tiny Machine Learning, bringing AI capabilities to ultra-low-power devices. In no way will TinyML suit all applications, yet it certainly marks a step into making AI accessible to many more devices.
- Field-Programmable Gate Arrays (FPGAs): FPGAs provide a dynamically reconfigurable architecture that lends itself very well to the breakneck evolution of AI. What is more, unlike in the case of GPUs and CPUs, FPGAs offer a designer the ability to quickly build and test neural networks, as well as adapt hardware to meet application-specific requirements. This flexibility is mission-critical in such high-stakes industries as aerospace and defence, medical devices, and others where the lifecycle of products is envisioned to be very long with the capability for fielding new algorithms.
- Graphics Processing Units: While endowing them with powerful parallel processing capabilities, the price to pay for energy efficiency and heat management is not cheap. However, they have remained as one of the favourites in many applications needing strong computational muscle, such as virtual reality and machine vision
- Central Processing Units (CPUs): Even with all the shortcomings of CPUs for parallel processing, they are embedded in many devices. Innovations such as Arm's Single Instruction Multiple Data SIMD architecture have increased the CPU's performance in running AI algorithms. However, they generally become slow with high power consumption compared to other computing devices like GPUs and FPGAs.
Conclusion
The shift from cloud-based AI to edge AI is dramatically changing how IoT systems process and utilise data. Edge AI enhances security, reliability, and flexibility by bringing AI processing closer to the source of the data and is, hence, perfect for a myriad of applications. However, implementation of edge AI will require properly considering hardware and software components and the unique challenges of deploying AI in resource-constrained environments.
As AI adoption escalates, this will only increase the demand for specialised hardware that solves the unique problems of edge computing. From matrix processors and in-memory processing to FPGAs and TinyML, these emerging technologies will define the next wave of edge AI solutions. In doing so, it enables application engineers to keep up with such technological developments, thereby empowering them to fully exploit AI at the edge in innovating and creating superior solutions.
With the fast-changing environment of AI, engineers and developers must stay up-to-date with new trends and technologies. If you'd like a deeper dip into AI, understand the building blocks of this field, and know how to put AI to work in real-world projects, head down to our AI Hub. Whether image classification, speech and gesture recognition, or conditional monitoring and predictive maintenance, AI Hub is fully catered to, providing you with a full set of product solutions, resources and expertise to help you unlock the maximum edge of AI.
Stay informed
Keep up to date on the latest information and exclusive offers!
Subscribe now
Thanks for subscribing
Well done! You are now part of an elite group who receive the latest info on products, technologies and applications straight to your inbox.
Read more on:
Artificial Intelligence at the Edge
Demystifying AI and ML with embedded devices
How to do classification using MAX78000 neural network accelerator
How to implement convolutional neural network on STM32 and Arduino
How to implement AR in process control application
Hello world for Machine Learning
Latest Trends in Artificial Intelligence
Deep Learning and Neural Network
AI and IoT: The future of intelligent transportation systems